Visitor II
September 15, 2020
Question
VIPER012HS reset on 230VAC
- September 15, 2020
- 2 replies
- 1111 views
Hi, I used the VIPER012HS controller following the non-isolated flyback scheme proposed by the tool design suit (which is the same by the datasheet) but after making the pcb I get a reset problem with the 230VAC mains voltage. I tried to input a direct voltage of 200VDC to the diode bridge and the controller works. over 200VDC the controller resets continuously. I am attaching the reference schemes (the scheme proposed by the tool design suite and my scheme). I tried the same scheme as mine with ltspice with all the correct models and it works correctly. I checked if there are any problems or shorts on the PCB and everything is ok. I can't figure out where the error lies. did I forget to evaluate any important specifications? thanks, Paolo