2021-10-27 12:51 PM
I use old Viper design software v2.24 for Viper53 design. Last time the program generate an error at startup (see attach). Reinstall, registry cleanup do not help to fix this error. Please, help.
Solved! Go to Solution.
2024-01-01 7:27 PM
I had the same problem with this program. Moreover, both in Windows 98 and in Windows 11. The reason turned out to be not in the new operating system, but in the display resolution being too high. Reduce the resolution and it will launch.
2021-10-28 12:35 AM
The screenshot shows that you are working with Windows 10 or later. However, this software was developed for a very old version of Windows, was out of date many years ago, is not compatible with Windows 10 anymore and throws tons of errors. Instead, STMicroelectronics switched to the online version eDesignSuite, which unfortunately does not support the VIPER53 anymore.
If you really want or have to use your software, you should run it on a computer or a virtual machine with an old Windows (not connected to the Internet for security reasons!).
Good luck!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter
2021-10-28 2:29 AM
I have desktop PC and notebook running the same versions of Win10 64. The 'overflow' problem present only on desktop PC. Some months earlier all works OK on desktop, so this problem can be resolved regardless to run to old PC.
2024-01-01 7:27 PM
I had the same problem with this program. Moreover, both in Windows 98 and in Windows 11. The reason turned out to be not in the new operating system, but in the display resolution being too high. Reduce the resolution and it will launch.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.