2010-09-17 4:52 PM
Un-symmetrically motor current - Design Problem with L6387e
2011-05-17 1:20 AM
Hello ierturk,
I don't know wether this is the reason of your problem, but from the scheme it looks like the boot capacitor is only 100pF which seemes to me to be a little bit low (consider that it musut keep the charge for two consecutive electrical steps). Can you try with 100nF (or even more up to 1uF)? May I ask you whether it is a sensored or sensor-less application? Regards, Billino