cancel
Showing results for 
Search instead for 
Did you mean: 

Totem pole PFC Control loop designs

AKUMA.5
Associate

The page number 46 current control design, The DPWM gain is given as 10^-3. The PWM Timer max value is 1000 for 72kHz freq for a clock of 72MHz. Then 1000 means 100% duty, 500 means 50% Duty.. etc. So the per unit duty (0 to 1) Shall be multiplied with a gain of 10^3 will give the digital pwm duty. So DPWM gain is 10^3 instead of 10^-3 ?

Correct me if my understanding is wrong !

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0