2025-09-10 1:30 AM
Hello,
I'm in the process of moving from MP1 to MP2 on my device. The latter, used STPMIC1 that suffered the startup problem as described in AN5861 and I had to go thru a re-design to include the latching circuit on my PCBA.
Can anybody confirm that this issue is gone for STPMIC25 that I will use for MP2?
Thanks in advance,
Daniel
Solved! Go to Solution.
2025-09-10 9:37 PM
Hello Daniel,
yes, STPMIC25 use different startup method and no issue if the input voltage is dropping fast.
Regards,
Vincenzo
2025-09-10 9:37 PM
Hello Daniel,
yes, STPMIC25 use different startup method and no issue if the input voltage is dropping fast.
Regards,
Vincenzo
2025-09-11 1:07 AM
Thanks a lot @Vincenzo , that is great news.