cancel
Showing results for 
Search instead for 
Did you mean: 

STPM32 IEC accuracy class reference

Franco Zampicinini
Associate II

Dear all, on STPM32 datasheet (DS10272 - Rev 12 ) there is this statement: "a meter using the STPM3x can reach IEC class 0.2 accuracy". On IEC standard, for meters, I only found class 0.2s specifications, where class 0.2 is only applied to current transformer. Please can you give me the IEC reference cited? Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hello! the datasheet in fact refers to Class 0.2 S of IEC 62053-22.

Best regards

Marilena

View solution in original post

5 REPLIES 5

Hello! the datasheet in fact refers to Class 0.2 S of IEC 62053-22.

Best regards

Marilena

Hi, many thanks! I wonder is you are able to add these information on the datasheet. Kind regards,

It is among the features in the first page, referred as IEC 62053-2x.

Best regards

Marilena

Got it. Maybe class 0.2s could help to avoid misunderstanding.

Thanks again.

Buon lavoro!

Thanks! we will add in the next datasheet release.

Buon lavoro!

Marilena