cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F100RBT6B 3V3 to Drive L6208 Stepper Motor Direct

michele
Associate
Posted on October 15, 2013 at 13:48

Hy, i must build a new board for control Stepper Motor. The pwm control logic and all,

is manage with new cortex STM like STM32F100RBT6B. I want an unique 3V3 logic

supply for all, is possible drive and receive all the logic signal control of the L6208 or similar

 stepper drive controller:  Clock, Reset, Half/Full, Cw ecc..  with 3V3 max high level signal ??

 Naturally the Motor have separated 40 Volt high power line voltage.

Thank you

Best regards
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Enrico Poli
ST Employee
Posted on October 21, 2013 at 10:51

Hi,

all the devices of the powerSPIN family are compliant with both 3V3 and 5V logic thresholds.

Regards

Enrico