cancel
Showing results for 
Search instead for 
Did you mean: 

SPI excample for the L9026

APneu.1
Associate

Hello,

ist there an SPI example available to control the L9026 for switching 8 solenoids?

Or even an example how to define the HEX command i have to send via SPI especial only to switch all 8 channels on and off.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Elena BRAMBILLA
ST Employee

hello,

sorry but examples of configuration via SPI are not available.

In case, if you want to switch on channels via SPI just write the relative bits in the register to "1": PWM_SPI, as reported in chapter 12.6 “SPI registers�?.

regards.

Elena