cancel
Showing results for 
Search instead for 
Did you mean: 

SCTWA70N120G2V Ron data

Kyle4
Associate

I want the specific Ron data corresponding to different VGS values (e.g., 8V–15V) when the MOSFET switch SCTWA70N120G2V is in the linear region.

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @Kyle4, to the community!

the SCTWA70N120G2V is manufactured using a technology, which, due to its structure, is targeted for switching applications. If this transistor is nevertheless operated in the linear region, there is a significant risk of hotspots forming in its drain structure, which will lead to avalanche-like destruction of the transistor.

For further and more detailed questions, I recommend contacting the FAE of the local distributor or sales office.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Kyle4, to the community!

the SCTWA70N120G2V is manufactured using a technology, which, due to its structure, is targeted for switching applications. If this transistor is nevertheless operated in the linear region, there is a significant risk of hotspots forming in its drain structure, which will lead to avalanche-like destruction of the transistor.

For further and more detailed questions, I recommend contacting the FAE of the local distributor or sales office.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.