cancel
Showing results for 
Search instead for 
Did you mean: 

problem with l298n

hamza_hamza11981
Associate II
Posted on July 14, 2009 at 16:08

problem with l298n

This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
hamza_hamza11981
Associate II
Posted on May 17, 2011 at 10:15

hi everybode

i have a problem with l298n ic

at this moment i burn 5 pes of l298n

i don no what is the problem

can anyone help me

motor current 0.5A

MOTOR VOLTAGE 24

hamza_hamza11981
Associate II
Posted on May 17, 2011 at 10:15

m using pwm at 500HZ or 2KH

AND the motor run at clockwise and ccw

plz see attached scematic diagram :D

enrico-dora-spa
Associate II
Posted on May 17, 2011 at 10:15

Hello hamza,

your application schematic seems ok.

I think you control motor current varying PWM duty-cycle, are you sure that motor current never exceed device absolute limits?

Are BR1 diodes of fast type? This is very important in order to correctly protect device.

Regards

Enrico POLI

Motor control team

hamza_hamza11981
Associate II
Posted on May 17, 2011 at 10:15

thanx for your reply

1-the max current is 0.5A(not more 0.5A)

2- the duty cycle at 100%

3-i m using usual bridge diode(selecon si)

not sottky diode****

I read the data sheet they prefare to be sottky DOIDE

4- i have 3 motors and 3 h_bridge**(plz see real scematic diagram)

and the three bridgs WAS burned

THEN

AA- is the capacitor (100nf) at Vs and Vss very impotant???

BB- can i add resistors to enable,and all inputs of the h bridge???

enrico-dora-spa
Associate II
Posted on May 17, 2011 at 10:15

I think device failure can be due by a lack of protection. During motor current recirculation external diodes should quickly clamp output pin voltage, this is why shottky diodes, or in general ''fast'' diodes, are recommended.

AA- The 100nF capacitors on VS and VSS are very important too. Sorry if I do not noticed they are not present in your schematic. I suggest to add an electrolytic capacitor to VS too (about 100uF should be enough).

BB- Sorry, but I not sure of the meaning of the question. Do you mean if you can pull-up L298 enable signals with a resistor instead to drive them through the micro?

[ This message was edited by: enrico-dora-spa.poli on 14-07-2009 10:08 ]

hamza_hamza11981
Associate II
Posted on May 17, 2011 at 10:15

thanx for your answer

i will do the changes and then tell you again

thanx agian :D