2025-11-13 5:37 PM - last edited on 2025-11-18 4:31 AM by SimonePradolini
Hello, (L6562DTR)I have encountered some problems when using this chip and hope to get some suggestions from you; ”The PF output voltage of 480V FC load is 0.7435“ The power input voltage is 250V-528VAC, with PFC+ flyback. The PFC BUS voltage is 760V, and the power output is 150W;When the input is 480VAC and the output is fully loaded, the THD is abnormal, ranging from 10% to 20% (5% for normal products), and at the same time, the PF value also drops and there is noise from the power supply
How can this problem be avoided