cancel
Showing results for 
Search instead for 
Did you mean: 

Operating temperature range of IC "STW4N150"

Pradeep2014
Associate

Can i know the minimum Operating temperature range of this IC "STW4N150"  

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Please note that the storage temperature must not be confused with the operating temperature and only refers to the storage of the device.
There is nothing to prevent operation at -30°C if the applicable parameters of the data sheet are observed.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Welcome @Pradeep2014, to the community!

you can use the STW4N150 down to -40°C, the data sheet also shows some graphs for -50°C.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks for the reply,

But the datasheet says that it has a operating temperature of max +150 and storage temperature has -55 to 150.

Can we operate in negative temperature "-30"?

Peter BENSCH
ST Employee

Please note that the storage temperature must not be confused with the operating temperature and only refers to the storage of the device.
There is nothing to prevent operation at -30°C if the applicable parameters of the data sheet are observed.

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.