cancel
Showing results for 
Search instead for 
Did you mean: 

Need help regarding STEVAL-ISA164V1

sohaib qamar
Associate II
Posted on April 17, 2018 at 16:36

Hi,

I got the STEVAL-ISA164V1 board from Digikey.

As far as the datasheet and online material shows, its an STNRG family of digital controller. Also, the IC mounted on the board is STNRG388A but when i open ST SMED configuration tool i'm unable to connect the board in STNRG category. The board connect successfully in STLUX385A category but i can't run any SMED. When i tried to connect the board using GUI software, it get connected but i can't see any Registers to manipulate.

I only see the Register restoreAfterReboot.

Secondly, when i tried to update the firmware of the board using en.stsw-stluxdev01 tool, its also not recognizing the board. I'm attaching the screenshot of error i get every time. (I'm giving the correct COM port shown in Device Manager).

Waiting for your positive response.

--

Regards

Sohaib

#stnrg388a #digital-power #steval-isa164v1
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.