cancel
Showing results for 
Search instead for 
Did you mean: 

LD39300 does not shutdown properly (output floats)

amer
Associate
Posted on July 16, 2013 at 13:10

Hello all,

  I have an issue with one of the linear regulators, LD39300 (PPAK), that I am using to provide 3.7V. When the INH pin is set low (with a jumper wire to ground), the output floats at about 1V.  On a previous version of the same PCB design, the output goes all the way down to 0V when INH is low.

  Has anyone come across an issue like this that may be to shed some light on a solution?

Thank you for your time and help.

A

Datasheet: 

http://www.st.com/web/en/resource/technical/document/datasheet/CD00150604.pdf

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0