cancel
Showing results for 
Search instead for 
Did you mean: 

LD39200PU33R

Skuma.151
Associate

Hi, recently we purchased LD39200PU33R Fixed voltage circuit.i have to give 5v input voltage but i get 4.7V..that datasheet mentioned 3.3V..expected voltage i didn't get..

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Skuma.151
Associate

Hi peter.. thank you for your reply..i got the output..The problem is capcitor value is not matching.

Regards

Sathish

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

The schematic looks OK and identical to the one in the datasheet. Please double-check if pin 2 (SENSE) is really connected to pin 1 (OUT).

If all pins are connected correctly, there is only a possible defect in the component, since the control transistor is fully turned on if the output shows 4.7V.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Skuma.151
Associate

Hi peter.. thank you for your reply..i got the output..The problem is capcitor value is not matching.

Regards

Sathish