cancel
Showing results for 
Search instead for 
Did you mean: 

L7987L multiple ICs in same board and how to synchronize them

Alejandro Bizzotto
Associate III
Posted on June 11, 2017 at 20:20

hi!

I'm making a DC-DC converter from +18~24V in to +/-13V, +5V out with at least 1A on each output. So far I have working the +/-13V@1.3A and I'm trying to synchronize them to have less noise. In the board I designed, I was just connecting the sync pins together but (after plug it) I realized they are referenced to a different levels of voltage so, no easy sync is possible here!

Is there a preferred way to do this? since the master will be the one with the highest frequency... how I should correct the levels if I don't know which one will be the master? Thanks in advance

#sync #dc-dc #l7987l
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0