cancel
Showing results for 
Search instead for 
Did you mean: 

L6480 absolute position counter value issue

Phlip Cornelissen
Associate III
Posted on January 15, 2018 at 10:45

Hi

The L6480 absolute position counter seems to count in multiples of 256 micro steps? When executing the move command with a 1000 micro steps or using the GoToDir command with a 1000 micro step value both generate a motion that ended in having a value of 256000 int the absolute position counter. When I reverse the direction the value is -256000 as expected, or should I say not expected! This count in multiples of 256 is a constant count and is not affected by the choice of micro stepping mode. may it be 1/8, 1/16 or 1/32 makes no difference!

Why is this? Is there a different setting or configuration for this? Any ideas on how fix this? I want to read the true number of micro steps and not in multiples of some value.

Best regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Kurtnelle
Associate III

Something is wrong in your code.