cancel
Showing results for 
Search instead for 
Did you mean: 

L6472 Step Clock Mode

bhushan4520
Associate II
Posted on January 16, 2018 at 13:18

Hello,I am using L6472 to control stepper motor. When i apply step clock mode command to L6472 , motor gets hold but during this opertion Motor shaft move by  1 to 2 degree , What  is the reason of shaft movement after applying STEPCLOCK mode command?

#step-clock-mode #stepper-motor #l6472
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Phlip Cornelissen
Associate III
Posted on January 17, 2018 at 10:23

The controller might zero to the nearest 'zero' electrical position, meaning the closest full step position, when switching to step clock mode. Its like when giving the hard stop command for the first time when the bridge was in high impedance mode, the motor switch to hold and the shaft makes a slight move as it locks to the nearest zero electrical position. To confirm this, try the following:

1 - Give the motor a move command in micro steps equal to the step mode to land on a full step position. So if your step mode is 1/8 micro steps per step then give a move command in multiples of 8, say 800. Now switch to step clock mode, it should not move or at least minimal. Read back the absolute position counter also to see if this is zeroed too!

2 - Give the motor a move command in micro steps in multiple of your step mode plus 1/3 of that, so if your step mode is 1/8 micro steps per step than give it a move command of say 802. Now switch to step clock mode. The motor will make a slight move in one direction, lets assume for now it is counter clock wise.

3 - Give the same move command as in step 2 but this time with 2/3 of the step clock mode, lets say 806 micro steps. Switch to step clock mode. If my theory holds, the motor should also make a slight move but this time in the opposite direction.