cancel
Showing results for 
Search instead for 
Did you mean: 

L6470 Power ON and RESET

chihiro_takahashi
Associate
Posted on June 20, 2014 at 07:29

Hi

I'm using L6470.

It works to move step motor a bit,when the Powered on.

The motor's coil  Voltage was high between  the RESET turn high and First SPI communication is started.(Almost 10ms?CPU's order)

I don't want to move a bit  when the IC powered on.

What is the problem about that?

?SW terminal is LOW when the RESET turn high.

#l6470-power-on-reset
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0