cancel
Showing results for 
Search instead for 
Did you mean: 

ECMF4-20A42N10 vs ECMF04-4HSWM10

qnguyen
Associate II

Hello,

 

Please confirm if ECMF04-4HSWM10 is possible replacement for ECMF4-20A42N10?  ECMF4-20A42N10 is in LTB status and we need replacement part with "recommended for new design" status.

Thanks,

Quynh

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @qnguyen, to the community!

You can consider the ECMF04-4HSWM10 as a possible replacement for the ECMF4-20A42N10, but it is neither a drop-in replacement (shorter package with a pitch of 0.4mm instead of the previous 0.5mm), nor are the technical data (e.g. frequency-dependent attenuation) absolutely identical.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome @qnguyen, to the community!

You can consider the ECMF04-4HSWM10 as a possible replacement for the ECMF4-20A42N10, but it is neither a drop-in replacement (shorter package with a pitch of 0.4mm instead of the previous 0.5mm), nor are the technical data (e.g. frequency-dependent attenuation) absolutely identical.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thanks Peter.

 

Quynh

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.