cancel
Showing results for 
Search instead for 
Did you mean: 

Did the L298HN ever have leads that were the same 5.28mm length ? The data sheet only shows one option where lead L6 is 2.38mm, and the other lead L5 is 5.28.

JTorr.7
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @JTorr.7​, to the community!

I have checked it again: the L298HN has had exactly this pin configuration since at least the year 2000, i.e. the inner pins are 2.38mm from the bottom edge of the device, the outer pins 5.28mm.

Does it help?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.