cancel
Showing results for 
Search instead for 
Did you mean: 

Clarification on STUSB4710QTR Configuration for 5V/5A Power Source

Digino
Associate

I just need some clarification regarding the STUSB4710QTR.

I'm designing a USB-C power source where a USB 2.0 hub will supply 5 V/5 A to a USB device. The connected device is a USB cellular modem, which typically draws a continuous 5 V/3 A, but requires brief pulses of up to 5 V/5 A during transmission.

I would like to configure the SEL_PDO pin for this application without using I²C. Could you please confirm if there is a default PDO profile that supports this, or if the SEL_PDO configuration allows selecting a 5 V/5 A contract directly?

I've attached a reference for your review.
Please let me know if everything looks in order or if you have any recommendations.

Thank you in advance for your support.

0 REPLIES 0