cancel
Showing results for 
Search instead for 
Did you mean: 

Can STUSB4710 act as a DRD?

MMSK
Associate

Hi,

 

Can PD Controller (STUSB4710) act as a DRD?

STUSB4710 - Stand-alone USB PD controller (with short-to-VBUS protection) - STMicroelectronics

I believe that STUSB4710 cannnot operate as DRD (Dual Role Data), and can only function as UFP.
If there is a way to operate it as DRD, please let me know how to configure it.

 

1 ACCEPTED SOLUTION

Accepted Solutions
Didier HERROUIN
ST Employee

Hello,

The STUSB4710 is a standalone chipset designed for SOURCE role only. As specified in the standard, at connection the Data role must be aligned with the Power role, so STUSB4710 is the Host (DFP). Then, the STUSB4710 does not support the Data Role swap, so it stays as the Host.
For information, some PCs (acting firstly as UFP) ask for a Data Role and they switch to DFP even if they do not receive any response. It is not really compliant to the standard.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Joe WILLIAMS
ST Employee

Hi MMSK

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly

 

Kind Regards

Joe

STMicro Support

Didier HERROUIN
ST Employee

Hello,

The STUSB4710 is a standalone chipset designed for SOURCE role only. As specified in the standard, at connection the Data role must be aligned with the Power role, so STUSB4710 is the Host (DFP). Then, the STUSB4710 does not support the Data Role swap, so it stays as the Host.
For information, some PCs (acting firstly as UFP) ask for a Data Role and they switch to DFP even if they do not receive any response. It is not really compliant to the standard.


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.