cancel
Showing results for 
Search instead for 
Did you mean: 

bSwitching ON/OFF two devices using two BTA06 but same Line

Engg Try
Associate
Posted on May 24, 2018 at 09:31

Dear All,

I have been working on a project where I need to Switch on Two devices using Two BTA06 controlled by Digitally Opto-Triac. Line and Neutral are same for both.

Attached is the schematic.

I have issue that when I swithch ON Triac 1 and keep Triac 2 OFF still I get 120V output on triac2 which should be zero.

However, switching OFF Triac 1 voltage is gone.

Can you please suggest what could I have missed?

#bta06-triac
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.