cancel
Showing results for 
Search instead for 
Did you mean: 

According to your non-disclosure agreement after successfully testing the controller & voltage multiplier cannot be used in released production... Would you have an equivalent to the STEVAL-IHM023V3 & STM32F769NI?

LHaac.1
Associate II

"This kit is not a finished product and when assembled may not be resold or otherwise marketed" c2014 STMicroelectronics - All rights reserved (UM1823)

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

What you mean is not an NDA, but the terms of use. And yes, all of our tools, including the STEVAL-IHM023V3, are only intended for evaluating the respective device and or starting your own development as quickly as possible.

I add the relevant section again here in full:

Notice applicable to Evaluation Boards not FCC-Approved

This kit is designed to allow:

  1. Product developers to evaluate electronic components, circuitry, or software associated with the kit to determine whether to incorporate such items in a finished product, and
  2. Software developers to write software applications for use with the end product.

This kit is not a finished product and when assembled may not be resold or otherwise marketed unless all required FCC equipment authorizations are first obtained. Operation is subject to the condition that this product not cause harmful interference to licensed radio stations and that this product accept harmful interference. Unless the assembled kit is designed to operate under part 15, part 18 or part 95 of 47 CFR, Chapter I (“FCC Rules�?), the operator of the kit must operate under the authority of an FCC license holder or must secure an experimental authorization under part 5 of this chapter.

So you are cordially invited to try out the kit extensively and to develop your software for it, but you have to derive and produce your own hardware from it in order to sell it as a final product.

Does it fully answer your question?

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Peter BENSCH
ST Employee

What you mean is not an NDA, but the terms of use. And yes, all of our tools, including the STEVAL-IHM023V3, are only intended for evaluating the respective device and or starting your own development as quickly as possible.

I add the relevant section again here in full:

Notice applicable to Evaluation Boards not FCC-Approved

This kit is designed to allow:

  1. Product developers to evaluate electronic components, circuitry, or software associated with the kit to determine whether to incorporate such items in a finished product, and
  2. Software developers to write software applications for use with the end product.

This kit is not a finished product and when assembled may not be resold or otherwise marketed unless all required FCC equipment authorizations are first obtained. Operation is subject to the condition that this product not cause harmful interference to licensed radio stations and that this product accept harmful interference. Unless the assembled kit is designed to operate under part 15, part 18 or part 95 of 47 CFR, Chapter I (“FCC Rules�?), the operator of the kit must operate under the authority of an FCC license holder or must secure an experimental authorization under part 5 of this chapter.

So you are cordially invited to try out the kit extensively and to develop your software for it, but you have to derive and produce your own hardware from it in order to sell it as a final product.

Does it fully answer your question?

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
LHaac.1
Associate II

Hi Peter,

In Summary, ST does not offer Production solutions but evaluation kits for software engineering applications?

If we are talking about STEVAL, DISCOVERY, NUCLEO and similar kits, then that's right, yes.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Or more specifically that the project is staffed at your end with SW / HW engineers capable of developing a commercial/production solution, that meets and passes certification testing, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..