cancel
Showing results for 
Search instead for 
Did you mean: 

STM32-Mat/Target problem with Simulink 2021a

ThorstenO
Associate II

Hi,

I was able to generate code for an STM32G474 with Matlab/Simulink 2020b. After an update to Matlab/Simulink 2021a code generation is no more possible. The only STM device I can choose is "ST10/Super10".

What can I do or when will a fix be available?

Thanks for help!

Thorsten

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amigo
Associate III

I am afraid that you are out of luck. STM32-MAT/TARGET is NRND (Not Recommended for New Design), and the last version, 5.6.0, is only recommended for Matlab R2018b. I already moved to other vendors' MCUs.

View solution in original post

2 REPLIES 2
Amigo
Associate III

I am afraid that you are out of luck. STM32-MAT/TARGET is NRND (Not Recommended for New Design), and the last version, 5.6.0, is only recommended for Matlab R2018b. I already moved to other vendors' MCUs.

邦平井.1
Associate II

Whether to use rtwbuild (model)

There is a build button when opening Embedded Coder from the Apps tab on the Simulink model