Read/Write to external EEPROM fails sometimes .What might be issue ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-19 8:57 PM
Hi,
I am using STM32L07XXX
I am reading/writing and external eeprom using I2C
" but I2C communication fails many time ". and system hangs
Does this function run needs to be atomic ?
But using __disable_irq and __enable_irq effects HAL_GetTick() ?
Can i enable only HAL_GetTick() ?
Or any other issue causing this ?
Following is code for writing to eeprom:
void write_eeprom_float(int mem_addr,float pdata, int size_write)
{
uint32_t time_start ;
time_start = HAL_GetTick();
while (HAL_I2C_GetState(&hi2c3) != HAL_I2C_STATE_READY)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
/* Check if the EEPROM is ready for a new operation */
time_start = HAL_GetTick();
while (HAL_I2C_IsDeviceReady(&hi2c3, EEPROM_ADDRESS, EEPROM_MAX_TRIALS, I2C_XFER_TIMEOUT_MAX) == HAL_TIMEOUT)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
/* Wait for the end of the transfer */
time_start = HAL_GetTick();
while (HAL_I2C_GetState(&hi2c3) != HAL_I2C_STATE_READY)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
if(HAL_I2C_Mem_Write(&hi2c3 , (uint16_t)EEPROM_ADDRESS,(uint16_t)mem_addr , I2C_MEMADD_SIZE_8BIT, (uint8_t *)&pdata, sizeof(pdata),1000)!= HAL_OK)
{
error_number = I2C_controller_EEPROM ;
/* Writing process Error */
Error_Handler();
}
time_start = HAL_GetTick();
while (HAL_I2C_GetState(&hi2c3) != HAL_I2C_STATE_READY)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
/* Check if the EEPROM is ready for a new operation */
time_start = HAL_GetTick();
while (HAL_I2C_IsDeviceReady(&hi2c3, EEPROM_ADDRESS, EEPROM_MAX_TRIALS, I2C_XFER_TIMEOUT_MAX) == HAL_TIMEOUT)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
/* Wait for the end of the transfer */
time_start = HAL_GetTick();
while (HAL_I2C_GetState(&hi2c3) != HAL_I2C_STATE_READY)
{
if((HAL_GetTick() - time_start) > 500)
break;
}
}
- Labels:
-
EEPROM devices
-
I2C
-
Interrupt
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-19 10:34 PM
>>Does this function run needs to be atomic.
Do you have multiple threads, or callbacks attempting to use the I2C bus?
You should arbitrate ownership via a mutex or semaphore, so each operation to each device can complete without interference.
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
‎2021-07-19 10:38 PM
No multiple threads and no callbacks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-07-20 6:09 AM
If you're only using blocking functions, the state should always be HAL_I2C_STATE_READY.
If HAL_I2C_IsDeviceReady returns anything other than HAL_OK, even a single time, the chip is misbehaving. Are there external pullups on the I2C lines?
When it fails, what fails, and what is the return value from the HAL function?