2017-03-07 11:44 AM
hello
i am working with STM32_MAT-TARGET in external mode i can generat project
help please
#stm32-mat-target #simulink #external #stm32-mat/target-matlabSolved! Go to Solution.
2017-03-09 1:30 AM
Hi
You can find attached the previous versionSTM32-Mat/TARGET V4.4.0 as you asked.
But, I recommendto you using the latest version of STM32-MAT/TARGETwhich contains enhancement asST maintains its supportonly for the last version of
STM32Mat/TARGET
available on the ST web.Imen
________________ Attachments : STM32MatTarget_4.4.0_setup.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HynU&d=%2Fa%2F0X0000000bCt%2Fm3YTaBi3ugz8uz4QSxa6BhBCZELVeStlZISxXk9Zy7w&asPdf=false2017-03-09 7:03 AM
I have copied your .ioc file in new folder and the project is successfully generated.
So, I think that the problem is related to your configuration setting with Keil.
2017-03-09 9:36 AM
i can generated a project with .ioc but the problem when i use simulink externel mode i cant generat project you can see the PDF
page 902017-03-10 9:07 AM
we aren't able to reproduce this error !
Please check that you are correctly configure Simulink Model Setting to use the correct parameters and the last version of CubeMx V4.20 (as mentioned in the attached document, in 'Simulink Model Setting' section)
2017-03-12 3:13 AM
thanks it is work
2017-03-12 6:03 AM
https://community.st.com/0D50X00009XkYEASA3
Mandatory Software :
matlab 2016 b
Keil version V 5.23
STM32CubMX 4.20
in the external mode : make sure thatHeapSize must behigher as possible.
make sure that the configuration of UART(Rx,Tx) in your stm32 it is connected to the USB (VCP_TX ,VCP_RX)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.