cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-H753ZI board Connect ADC inputs to GND, the readings are varied between -15 - +15

RongShengWang
Associate III

Nucleo-H753ZI board. ADC1 configurations: INPUT: SINGLE-END

Sample clock rate = 5Mhz

Sample rate = 10Khz,

Sample Time = 16.5 cycles,

Resolution = 12-bit

Scan 256 times

Connect the defined two ADC input channels to GND.

The 256 readings FOR EACH INPUT are varied between (-15 - +15), more or less, while they should be read as zeros.

Question: Can it be fixed How to fix it?

Could you do the same test to confirm it?

Thanks,

 

Rong

12 REPLIES 12

The problem was due to the longer wiring on the Eva board. After shortened the wires, the data read out is between

0-2 now. Nothing else was wrong.

Case closed.

I have the NUCLEO-H755 and I get between 0-2 with oversampling. Without oversampling, I get value between 0-4.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

The problem was due to the longer wiring on the Eva board. After shortened the wires, the data read out is between

0-2 now without oversampling,. Nothing else was wrong.

Case closed.