2022-05-30 2:55 AM
I have found that under the windows 11 control panel the ST-Link driver is not correctly recognized. Please see the attached picture about this.
There were no problems of this sort on windows 10, it only occured on windows 11. I tried to reinstall the driver without success.
2022-05-30 3:21 AM
Please right click on the ST-LINK and open properties. What is the error number?
Do you remember what exactly you did to reinstall the driver?
2022-05-30 3:33 AM
It says that the drivers are not installed (code 28), but i performed the installation as requested with IAR Embedded Workbench that has a specific section for the drivers installation.
I've also tried to download them from the net and install them myself, but the result was the same.
2022-05-30 7:13 AM
@GParr.1 "i performed the installation as requested with IAR Embedded Workbench that has a specific section for the drivers installation"
If you've followed IAR's own documentation, and that hasn't worked, you should be taking that up with IAR.
Does the St-Link work with any other IDE(s) ?
2022-05-30 8:54 AM
The installation worked without any problems on windows 10 and i was able to upload programs and work on the STM32F401 MCU without any errors showing up.
Recently I had to switch to a computer with windows 11, i re-installed the IAR program from scratch like i did the first time on windows 10. IAR still works perfectly on the new OS, but the STM32F401 doesn't.
I haven't tried it with any other IDEs because i was told to use IAR for my projects.
2022-05-31 12:23 AM
@GParr.1 Try to install the driver manually.
Download the driver package from
https://www.st.com/en/development-tools/stsw-link009.html
and unzip into some directory.
Then right click on the ST-LINK, select Install, Browse for drivers... and point it to the unzipped directory.
If new uninstalled devices show on, repeat.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.