2026-01-16 4:04 AM - last edited on 2026-03-02 3:03 AM by Imen.D
Hello, I need a clear step by step guide on how to set up Pnucleo lrwan 3 end node and gateway and connect both to the loriot server. currently I have issues communicating with my END node using the AT command via terminal.
My other issue is that; the PNUCLEO lrwan 3 antenna is 480MHz, but when I check the paramaters of the device using terminal, I discover that the frequency is EU-868MHz, so now I have to reconfigure the device tp the right frequency, how do I do this. I have consulted the UM2587 material but it does not appear to be so clear to me.
2026-01-16 4:58 AM
Note that the P-NUCLEO-LRWAN3 is Not Recommended for New Designs (NRND), and has been for a long time now:
And the Gateway was never suitable for deployment.
See:
2026-01-19 1:45 AM
Thank you for the clarification about the P-NUCLEO-LRWAN3 being NRND and the gateway not being suitable for deployment. I understand that this kit is not recommended for production use.
However, I am currently using this kit strictly for learning and laboratory testing of LoRaWAN, and I would really appreciate some guidance on how to correctly complete my setup. Does this mean I can not use the P-NUCLEO LRWAN3 ?
2026-01-19 2:12 AM - edited 2026-01-20 4:07 AM
If you look in the linked thread, the Gateway is actually Obsolete.
The RF part was by RisingHF - I don't know if they have any support for it any more.
I think you'd be better off getting a separate Gateway - or, perhaps, check if you are already in-range of a public Gateway...
PS:
RisingHF support: http://risinghf.com/en/enWIKI/index.html
RisingHF contact: http://risinghf.com/en/enabout/#plate4
GitHub: https://github.com/risinghf