cancel
Showing results for 
Search instead for 
Did you mean: 

Will it work (SCI 1Mb Baud Rate)

nirn
Associate II
Posted on November 05, 2003 at 12:15

Will it work (SCI 1Mb Baud Rate)

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
nirn
Associate II
Posted on November 05, 2003 at 08:11

I'm trying to get the Maximum Baud Rate possible from the SCI -

According to the Data Sheet its 500k.

Look at my configuration and tell me if it's gooing to work -

The configuration is for 1M Baud Rate with 16MHz CPU osc.

SCIBRR = 0x00

SCIEPRP = 0x01

SCIETPR = 0x01

As you can see I'm using the extended mode of the SCI.

What do you say ?
sjo
Associate II
Posted on November 05, 2003 at 12:15

500K is the maximum the sci may be set, this is stated in the datasheet for the device.

On the newer devices it is possible to reach the maximum baud rate by just using the conventional Baud Register - TR & RR=1, PR=1.

The older devices have to use the extended Baud Register. (ST removed the /2 from the BRR frequency).

Regards

sjo

[ This message was edited by: on 07-11-2003 05:37 ]