cancel
Showing results for 
Search instead for 
Did you mean: 

what is the function of the Clock Configuration Register (ENET_CCR)

sunyuanling1022
Associate II
Posted on March 16, 2007 at 04:53

what is the function of the Clock Configuration Register (ENET_CCR)

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
sunyuanling1022
Associate II
Posted on May 17, 2011 at 09:39

Hello!what is the function of the Clock Configuration Register (ENET_CCR),I can not find the code refer to the register in the ENET library.who can help me ?Thank you!

amira1
Associate II
Posted on May 17, 2011 at 09:39

Hi sunshan,

It's not important to configure ENET_CCR register because the DMA units are located only on the AHB bus and not on the APB.In fact, this register have its reset value (HCLK=PCLK).

With best regards,

mirou

sunyuanling1022
Associate II
Posted on May 17, 2011 at 09:39

Thank you!can you look at the message which title is ''the perplexity about the MAC/DMA Controller with DMA''.