cancel
Showing results for 
Search instead for 
Did you mean: 

Vstby value

mymail2000
Associate
Posted on July 07, 2005 at 07:22

Vstby value

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
mymail2000
Associate
Posted on July 07, 2005 at 06:54

Hi

According to the datasheet, the lowest stand-by voltage Vstby = 4.0V (without RTC and 32kHz oscillator).

On the final version of ST10F276, could the Vstby be lower than 4V?

Thanks

najoua
Associate II
Posted on July 07, 2005 at 07:22

Hi,

No the Vstby could not have a value lower than 4V. I think you ask this because you want to use a battery to back up the device in standby mode and that the batteries are usually 3.3V but unfortunatly this is not possible.

Regards,