cancel
Showing results for 
Search instead for 
Did you mean: 

vnd7e025 - input capacitance limits

JBrin.1
Associate

Very interested in your vnd7e025. Datasheet doesn't have load capacitance limits - but states its rated for "capacitive and inductive loads". Can you please provide details about maximum capacitance and/or inrush magnitude and duration allowable for safe non-damaging operation?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

As you probably know, there may be a large current peak with large capacitive loads. The VND7E025AJ is able to easily handle that and to drive inductive and capacitive loads due to the internal protection features:

  • for capacitive loads: current and power limitation
  • for inductive loads: negative voltage clamp

Because of these protective functions, it is not necessary to specify maximum values for e.g. inrush current.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.