cancel
Showing results for 
Search instead for 
Did you mean: 

VM reg

jgil
Associate II
Posted on June 19, 2003 at 10:29

VM reg

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jgil
Associate II
Posted on May 17, 2011 at 11:54

Hello,

We are trying to implement a debug system of the code for upsd323x . In that we have mapped boot flash as code &

primary flash as data in a combined space mode.

How should set the initial value of the VM register using the PSDsoft express? I don't find the option in the PSD menu configuration.

Thanks in advance for any comments.

Regards,

Jokin
simonharrison9
Associate II
Posted on May 17, 2011 at 11:54

Hi,

The initial VM setting is derived from the Define MCU/DSP and PSD section

Step 3 - Select PSD configuration

The lower two pulldown options select where the Main and Secondary flash should be , DATA, PROGRAM or BOTH

To select memory addressing, this follows the pin definition page.

Once the pin definitions are defined, click Next>>

This will take you through page definition and addressing (Chip Select Equations)

Please see

http://www.st.com/stonline/books/pdf/docs/9439.pdf

for a full guided version of PSDexpress

regards,

Simon

[ This message was edited by: sjh on 12-11-2003 16:22 ]