cancel
Showing results for 
Search instead for 
Did you mean: 

USB IAP problem

jagtap
Associate II
Posted on November 03, 2008 at 01:52

USB IAP problem

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jagtap
Associate II
Posted on May 17, 2011 at 11:52

Hello,

I am develop an application on uPSD3454EV for In-Application Programming (IAP) using USB. i use our own USB drivers developed on WinDDK and well tested on ARM system, firmware for uPSD3454EV for both boot loader and application is written in the C language and complied using keil uVision3 compiler and PC side software is developed in Visual C.

I am face problem regarding its reliability means if we download firmware in the uPSD3454EV controller 50 times using my USB IAP it is ok ( means full downloading is complete ok and device work functionally ok ) nearly 25 times only and other times it is failed. i test this on 4 to 5 different PC but i get same result.

And when downloading is not ok it stop download at somewhere and pc side software give me error.

Error: A device attached to the system is not functioning.

please give me documents if anyone find such problems and solution on it, or some extra care which i want to take which is not given in datasheet of uPSD34xx, or give some probable reason because of it may happen.

Waiting for your replay.

Thank You.

Somnath H. Jagtap