cancel
Showing results for 
Search instead for 
Did you mean: 

URGENT PLEASE ( XDATA DATES)

ricardof
Associate II
Posted on July 25, 2005 at 05:43

URGENT PLEASE ( XDATA DATES)

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
joseph2399
Associate II
Posted on May 17, 2011 at 12:07

Please double check that you have selected the battery backup option in PSDsoft express and that this option has been programmed into the device.

ricardof
Associate II
Posted on May 17, 2011 at 12:07

If in my board I have a battery of 3,3 volts. ( uPSD3312) when I switch off the supply the dates recorded in xdata remain or dissapear. Because the problem that I have if when I switch off and switch off quiclky the dates in xdata have changed and my application programme doesn´t work Ok.

ricardof
Associate II
Posted on May 17, 2011 at 12:07

the pin PC2 is programmed like vstby and has been programmed like SRAM standby voltage input, I think the pin is well programmed, so at this moment I don´t know what it´s happenning? Tanks for your help

danielh1
Associate II
Posted on May 17, 2011 at 12:07

There are 3 possible causes to your problem:

1 - Some defect in your battery backup circuit (or in the battery itself).

2 - Your main supply is RFI sensitive.

3 - A software problem, like the one suggested by Phaze.

Assuming that you have checked your software and eleminated possibility 3, try the following:

1 - Switch off the power SMOOTHLY, by unplugging the AC cord for example.

2 - Discharge the main capacitor just after the AC rectifier, using a small resistor (about 100 ohms). Don't short it: this would cause a spike.

3 - Wait a minute an switch on again the power. Are your data ''desprogrammed'' or not?

Daniel