cancel
Showing results for 
Search instead for 
Did you mean: 

There is any problem connect NC pin of M24C04 to ground? I intend replace a ATC24C Microchip to M24C04 STm.

Rogerio
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

OK, in this case you can leave NC connected to GND, there is no internal connection.

But keep in mind that the M24C04 has a smaller EEPROM area than the AT24C32E.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
Peter BENSCH
ST Employee

Maybe that was a typo and you meant the AT24C04C?

If this is the case, then AT24C04C and M24C04 have the same pinout, i.e. both have NC on pin 1.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Rogerio
Associate

AT24C32E-SSHM-T have pin 1 ,2 and 3 to address. In this case all pins to ground.

OK, in this case you can leave NC connected to GND, there is no internal connection.

But keep in mind that the M24C04 has a smaller EEPROM area than the AT24C32E.

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.