cancel
Showing results for 
Search instead for 
Did you mean: 

STVD7 & DVP3: I2C not defined for ST72321AR6

ppoulin
Associate II
Posted on July 30, 2004 at 13:59

STVD7 & DVP3: I2C not defined for ST72321AR6

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
ppoulin
Associate II
Posted on July 07, 2004 at 13:18

When running Debugger on DVP3 with STVD7 on a ST72321AR6, I get no I2C running. Looking in MCU Configuration, I see there is no I2C defined from 0x18 to 0x1E in the Config map.

Is there any way I could be able to config that MCU for I2C running ?

Thanks
alain2399
Associate II
Posted on July 09, 2004 at 07:33

Hello,

It seems that you are right, the I2C registers are correctly defined in the SFR descriptions but the memory area is declared as NEM (Non Existant Memory) in the maping. The error exists for the st72321 (A)R6, st72521 (A)R6, st72521 B(A)R6.

The error does not exists on the EMU3. This will be fixed in the next release of STVD7.
ppoulin
Associate II
Posted on July 09, 2004 at 17:22

Opening the mdb file in ..\dvp3\config and correcting the appropriate lines in the memory area map table would probably correct the problem.

alain2399
Associate II
Posted on July 15, 2004 at 07:01

Be aware that any change to the files of STVD7 after installation can cause severe problems and can be done only at your own risks.

[ This message was edited by: Alaini on 15-07-2004 10:31 ]
emmanuel23
Associate II
Posted on July 30, 2004 at 13:59

The patch is now available on this web site

http://mcu.st.com/mdtfiles/1091199515.zip

This patch can be installed on release 3.0.1 only.