2026-05-11 6:34 AM - last edited on 2026-05-11 8:15 AM by Peter BENSCH
Hi,
I'm building a DC-DC converter with a USB-C output using an ESP32 and a STUSB1602 configured as a fixed 5V/3A Source (no PD stack).
The problem: when I plug a USB-C cable into my receptacle connector, the FSM jumps directly from Unattached.SRC (0x08) to ErrorRecovery (0x13) without going through AttachWait.SRC (0x09) or Attached.SRC (0x0A). No alert is generated on the ALERT pin, and CC_DETECTION_STATUS (0x0E) stays at 0x00 the whole time — the chip never seems to detect Rd on CC1 or CC2, even though I physically measure a voltage drop to ~0.3V on CC1 when plugging.
Hardware setup:
STUSB1602 as Source, I²C 0x28
USB-C receptacle
CC1/CC2 connected directly to the chip, no external resistors
VBUS_SENSE upstream of the MOSFETs (connector sees no VBUS before attach)
Software configuration:
0x28 POWER_ROLE_CTRL = 0x00 → Source
0x18 PD_ROLE_CTRL = 0x90 → Rp=3A
0x20 MONITORING_CTRL = 0xB0 → VBUS+VCONN monitoring
0x22 VBUS_RANGE_MONITORING = 0x66 → OVP/UVP ±20%
0x0C ALERT_STATUS_MASK = 0x00 → all alerts unmasked
What I captured at the moment of ErrorRecovery:
CC_DET (0x0E) = 0x00 → no Rd detected FSM (0x11) = 0x13 → ErrorRecovery 0x0F MONITORING_TRANS = 0x04 → VBUS_VSAFE0V transition (VBUS dropped below 0.8V) 0x12 HW_FAULT_TRANS = 0x00 → no hardware fault 0x13 HW_FAULT_STATUS = 0x40 → VPU_VALID=1, no fault 0x0B ALERT_STATUS = 0x00 → no alert
The only clue I have is the VBUS_VSAFE0V transition on 0x0F, suggesting VBUS drops below 0.8V at the moment of plug-in, which might be triggering ErrorRecovery.
But I'm not sure if that's the cause or a consequence.
What I've ruled out:
I can't find any documentation listing the exact conditions that cause the STUSB1602 to enter ErrorRecovery.
Thanks
2026-05-11 8:15 AM
Welcome @remi_l, to the community!
As the STUSB1602 has been discontinued, there is no longer any documentation available for it either, so unfortunately STMicroelectronics can no longer help you. The only possible source of support might be a helpful user here in the community.
I’m very sorry I can’t give you a more positive answer.
Regards
/Peter
2026-05-11 11:07 AM
Okay, I understand.
I hope someone in the community will be able to help me.
Thank you anyway!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.