cancel
Showing results for 
Search instead for 
Did you mean: 

STR912 IRQ woes (GCC/Eclipse/OpenOCD)

frikkie
Associate
Posted on June 02, 2008 at 09:26

STR912 IRQ woes (GCC/Eclipse/OpenOCD)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
frikkie
Associate
Posted on May 17, 2011 at 09:53

Hi ppl,

I've been playing with GCC (4.3) (newlib)/Eclipse/OpenOCD to try and get a

timer interupt working. I've managed to see in the VIC0 interrupt

status registers that the interrupt flag for timer0 is set on a ''TOF''

(timer overflow) of the timer.

The problem is that the CPU doesn't branch to execute my interrupt service routine. Placing a breakpoint in the startup code at 'LDR PC, [PC, #-0x0FF0] doesn't get hit at all.

Can anybody please give me some pointers on what else to look at to determine why the interrupt isn't executed?

I've attached the source code of my project in ZIP format.

Regards,

-Frikkie Thirion

//Startup code snippet:

Vectors:

LDR PC, Reset_Addr /* 0x0000 */

LDR PC, Undef_Addr /* 0x0004 */

LDR PC, SWI_Addr /* 0x0008 */

LDR PC, PAbt_Addr /* 0x000C */

LDR PC, DAbt_Addr /* 0x0010 */

NOP /* 0x0014 Reserved Vector */

LDR PC, [PC, #-0x0FF0] /* Vector from VicVECAddr */

LDR PC, FIQ_Addr /* 0x001C FIQ has no vector! */

Reset_Addr: .word Hard_Reset

Undef_Addr: .word Undef_Handler

SWI_Addr: .word SWI_Handler

PAbt_Addr: .word PAbt_Handler

DAbt_Addr: .word DAbt_Handler

.word 0 /* Reserved Address */

IRQ_Addr: .word IRQ_Handler

FIQ_Addr: .word FIQ_Handler

Undef_Handler: B Undef_Handler

SWI_Handler: B SWI_Handler

PAbt_Handler: B PAbt_Handler

DAbt_Handler: B DAbt_Handler

IRQ_Handler: B IRQ_Handler /* should never get here ... */

FIQ_Handler: B FIQ_Handler

In main():

----------

HAL_isr_init();

HAL_isr_init_timer0();

//What is the contents of the interrupt service routine?

wI=VIC0->VICx_ISR;

if ( (wI&0x10) == 0x10)

{

wI=0; // Place to put a breakpoint - (This gets hit in GDB)

}

HAL_isr_init():

---------------

u32 wI;

//Enable SCU clock to peripheral:

//Set bit[5] in SCU Peripheral Clock Gating Register 0

wI = SCU->PCGR0;

wI |= 0x00000020; //[5] = VIC

SCU->PCGR0=wI;

//Take peripheral out or reset:

//Set bit[5] in SCU Peripheral Reset Register 0

wI = SCU->PRR0;

wI |= 0x00000020; //[5] = VIC

SCU->PRR0=wI;

//Assign a default function routine to the DVAR, for spurious

//interrupts

VIC0->VICx_DVAR=(u32)HAL_isr_default_VIC0_isr;

VIC1->VICx_DVAR=(u32)HAL_isr_default_VIC1_isr;

HAL_isr_init_timer0()

---------------------

// Interrupt enable: VICx_inter, p118

wI=VIC0->VICx_INTER;

wI|=(1<

VIC0->VICx_INTER=wI;

// Interrupt select register, p118

wI= VIC0->VICx_INTSR;

wI&=~(1<

VIC0->VICx_INTSR=wI;

// Vector address i registers

// Set 'vector address' to Timer0's ISR

VIC0->VICx_VA0R=(u32)&HAL_TIM0_isr;

// Vector control i registers, p122

wI=4; //[3..0] = These bits select the interrupt source for the

//vectored interrupt.

wI|=(1<

VIC0->VICx_VC0R=wI; // Select to match VIC0.4 for timer0