cancel
Showing results for 
Search instead for 
Did you mean: 

STR755 USB pins

pete3
Associate II
Posted on June 15, 2007 at 14:01

STR755 USB pins

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
pete3
Associate II
Posted on June 11, 2007 at 10:56

Hi chaps,

The STR755 doesn't have a USB peripheral. In the LQFP100 package, there are USB pins. Does anyone know their function when there's no USB peripheral in the device? I presume this carries through to the STR752 too.

Cheers,

Peter

kaouther
Associate II
Posted on June 13, 2007 at 11:36

Hello,

For the 64 pin package, pins 41 and 42 are shared with USB and CAN. depending on device part number. For example, the STR752FRx only CAN is available. The 41& 42 pins are mapped to P0.15/CAN_TX and P0.14/CAN_RX.

In addition, the non available pins on LQPFP64 and LFBGA64 packages are internally tied to low level.

Regards.

pete3
Associate II
Posted on June 14, 2007 at 06:47

Thanks coucou. Do you have any information on the LQFP100 package?

Regards

kaouther
Associate II
Posted on June 15, 2007 at 09:00

Dear peterwrigley,

For the LQFP100 package, when there's no USB peripheral in the device as STR755FVx part number, the corresponding USB pins should be left unconnected and not used.

Thanks.

pete3
Associate II
Posted on June 15, 2007 at 14:01

Thanks coucou, that's exactly what I was after!