cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F276 ADC conversion and XADC

p-alain
Associate II
Posted on July 14, 2005 at 05:02

ST10F276 ADC conversion and XADC

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
p-alain
Associate II
Posted on July 13, 2005 at 09:32

Hello

I use a ST10F276 and Keil. I have configure my ST10 like the ST10F269. Here you can see my configuration. the IT_mesures_analogiques run every 500us.

ADCIC = (14<

SRCP0 = (int)(&ADDAT);

ADCIE = 1;

NB_ADCCH = 1;

ADC_0 = 0;

void IT_adc (void) interrupt ad_trap using registres_ad_trap

{

value_0 = adc_value[NB_ADCCH-1-ADC_0];

}

void IT_mesures_analogiques (void) interrupt t6_trap using registres_t6_trap

{

ADCON = (0x0020|(NB_ADCCH-1)); // Auto scan

// single conversion of NB_ADCCH channel

DSTP0 = _sof_(adc_value);

PECC0 = 0x0200|NB_ADCCH;

ADST = 1; // ADC start bit

}

I have 3 problems :

1.With this configuration I have the ad interrupt but the value_0 = 0 between 0Volt

and 5 Volt.

2.If I add 1 channel :

NB_ADCCH = 2;

ADC_0 = 0;

ADC_0 = 1;

I have i watch dog interrupt and a reset.

3.the 3rd problem is how to do to have an uto scan single conversion of 24 channels (16 ADC + 8 XADC).

Thank you.