cancel
Showing results for 
Search instead for 
Did you mean: 

SPI MODE

tech4
Associate II
Posted on July 25, 2003 at 11:32

SPI MODE

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
tech4
Associate II
Posted on July 25, 2003 at 11:16

The SPIF bit seems not to be reseted after a write to the SPIDR ?

My address is sent first OK, but the following data seems not to be sent ... why ???

bset SS_SPI ;SS/ = 1 sélection RTC

ld A,#7Ch ;SPI enabled and interrupt disabled - Serial Clock at Fcpu/4

ld SPICR,A ;SCK is at high level in idle state and

;The second clock transition is the first capture edge

ld A,#03h ;SPI output enabled - SS/ external pin = CE RTC

ld SPICSR,A ;SSI = 0 => Slave selected

ld A,SPICSR ;Reset bit SPIF

ld A,#8FH ;Sélection adresse contrôle register

ld SPIDR,A

att_spi0

btjf SPICSR,#7,att_spi0 ;Wait until end of transmission

ld A,SPICSR ;Reset bit SPIF

ld A,#00H ;Initialisation du registre de contrôle à 0

ld SPIDR,A

sjo
Associate II
Posted on July 25, 2003 at 11:32

To clear the SPIF you have to read or write the SPIDR not the SPICSR after an access to the SPICSR. I read the SPIDR as it covers both slave and master mode.

Taken from datasheet:

Clearing the SPIF bit is performed by the following

software sequence:

1. An access to the SPICSR register while the

SPIF bit is set

2. A read to the SPIDR register.

Hope this helps

SJO