2008-07-21 3:11 AM
RESET_IN trigger will cause which LVD State?
2011-05-17 12:54 AM
Hi,
I want to use the LVD functionality to hold up the contents of RAM to enable a Warm Start feature. From my understanding, LVD must trigger a shutdown mode for the LVD Register to read a 1 to indicate RAM was held up. What happens if LVD is not triggered but an external event triggered RESET_IN instead? Will the RAM contents stay intact in this condition and what should the LVD bit read? Is there any indication that the RESET_IN pin was triggered? Thanks Mark