cancel
Showing results for 
Search instead for 
Did you mean: 

Replacement or upgrade of ST62T42BQ6 Requested

pwdandekar
Associate
Posted on November 28, 2005 at 11:29

Replacement or upgrade of ST62T42BQ6 Requested

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
pwdandekar
Associate
Posted on September 30, 2005 at 06:01

Hello All,

I am looking for a replacement for ST62T42BQ6 chip. This is 64 pin PQFP64 package.

Some of the salient requirements are OTP or cheapest varient, 8K ROM, 192 bytes RAM, 6 channel 8-bit ADC, TWO 8-bit timers with 7-bit prescaler and 40 x 4 LCD segment driving lines.

If anybody is using any low-cost ST product which meets all of the above specs, please suggest.

Thanks in advance.

vikas2
Associate II
Posted on September 30, 2005 at 09:17

Replacement for ST62T42BQ6 is ST7 microcontrolers. According to your need you can select the appropriate one from the following link

http://mcd.rou.st.com/modules.php?name=mcu&file=familiesdocs&FAM=15#Datasheet

You will find it easily rather with more accurate set of features except the LCD segment driving lines e.g . For that i will suggest you to go for software implemented LCD driver with full explanation in AN1048(available at link www.st.com/stonline/books/pdf/docs/6292.pdf ) It is very efficient in terms of speed and memory requirements.