cancel
Showing results for 
Search instead for 
Did you mean: 

[q]Ask about developing usb module at uPSD3234A

byounghoon_koh
Associate II
Posted on April 29, 2003 at 14:46

[q]Ask about developing usb module at uPSD3234A

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
joseph2399
Associate II
Posted on May 17, 2011 at 11:53

In the attached zip file a document called, USB Demo App. Structure.doc, explains how to setup the USB interface. Also included in the zip file is the USB IP driver source code and the PSDsoft project files for the ST's DK3200 Eval board, it should help you to get your USB IP development started.

byounghoon_koh
Associate II
Posted on May 17, 2011 at 11:53

Hello guys,

Now I'm developing a system with uPSD3234A. This MCU deals usb

module by HID(Human Interface Device). Can anyone tell me the

flowchart of developing the usb module program? If some test board

is needed just do it with DK3200 demo board.(AN15pdf - this

includes total circuit diagram.)

I need your help...

Best regards,

Byounghoon

simonharrison9
Associate II
Posted on May 17, 2011 at 11:53

Hi,

The file seems to be corrupted, can you re-post?

Simon
jacques
Associate II
Posted on May 17, 2011 at 11:53

sjh,

Please try your download again, the file is not corrupted.

There was a problem with the code of the page.

byounghoon_koh
Associate II
Posted on May 17, 2011 at 11:53

Hello,

Thanks for the file however, I had it already. I need more detail approach. If you don't mind, would you let me show the flow chart

for the connect procedure between firmware and windows application?

I studied all registers of firmware but I can't build them in order to operate.

Best regards,

Byounghoon

dk5ug
Associate II
Posted on May 17, 2011 at 11:53

Hello,

you are a professional, aren't you?

The supplied sources describe the USB-interface well

and sufficient.

They work - once the hardware does. This problem has

been solved; see elsewhere in this forum.

Besides - I highly recommend the study of general USB-

literature. You won't understand the handling of USB by

simply reading sourcecode.

Regards

[ This message was edited by: Nickname on 21-04-2003 13:48 ]

byounghoon_koh
Associate II
Posted on May 17, 2011 at 11:53

Thanks for an advice. I'll dig the source more as you said.

I completely agree with you that it is very hard to deal the

USB module with sufficient knowlege base of USB. I'll study USB

more first.

Thanks,

Byounghoon

simonharrison9
Associate II
Posted on May 17, 2011 at 11:53

Quote:

On 2003-04-18 15:43, dag wrote:

sjh,

Please try your download again, the file is not corrupted.

There was a problem with the code of the page.

Many thanks dag,

Simon