cancel
Showing results for 
Search instead for 
Did you mean: 

Protecting ICCCLK & ICCDATA

brian4
Associate II
Posted on April 16, 2005 at 05:23

Protecting ICCCLK & ICCDATA

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
brian4
Associate II
Posted on April 15, 2005 at 10:22

I have an application where I need to encapsulate the ST7 Lite, I have a connector on the PCB for my I/O.

I would like to bring out to the same connector the ICCCLK & ICCDATA lines so I can programme & debug with my Indart STX programming tool.

Any advice on how to protect these lines from over voltage and short circuit etc. i.e. what seies resistance can I place in these 2 lines 2 allow the ICP to operate but allow protection to my ST7

Regards

Brian

[ This message was edited by: BrianM on 15-04-2005 13:56 ]

venkateswara
Associate II
Posted on April 16, 2005 at 05:23

Hi,

You have to connect a 4.7K or more value resistor only if you are using the pins for input mode in your application. If you are using them for output, no need of any resistors. you can see the indart user manual.

Hope this helps.

bye

venky