cancel
Showing results for 
Search instead for 
Did you mean: 

Programming of ST7FLite

rolf_mussgnug
Associate II
Posted on October 13, 2004 at 08:20

Programming of ST7FLite

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
rolf_mussgnug
Associate II
Posted on October 13, 2004 at 05:37

I'm searching for a ''DLL'' to include it inside WINDOWS for programming a ST7FLite over a needle adaptor.

ldefend2
Associate II
Posted on October 13, 2004 at 08:20

SofTec Microsystems has developed IPL-ST7, an interface library (DLL) which works together with any instrument of the inDART-ST7 series and inDART-STX for ST7 series and allows user-written Windows applications to automatize programming sessions.

The IPL-ST7 Programming Library is a DLL which includes all of the low-level functions that allow users to set up the instrument and perform, from within their own Windows application, most of the programming commands and functions of the DataBlaze user interface.

The IPL-ST7 Programming Library contains C written routines, and can be used to interface the instrument from within, for example, a Microsoft Visual C or Visual Basic application, as well as any other programming language that supports the DLL mechanism.

Hope this helps...

Luca

http://www.softecmicro.com

[ This message was edited by: Luca_Defend on 13-10-2004 11:54 ]